SPRADI0A July 2024 – November 2024
The Embedded Coder tool allows the flexibility to profile a part of the application code, multiple blocks in the application code or the complete application code using Simulink. There can be multiple ways to profile the code generated by MATLAB – Processor-in-loop method on Simulink, C2000 Timer, general-purpose input/output (GPIO)-based profiling and the CCS clock profiler tool. While there is no notable difference in terms of the profiling data, there might be small differences due to different approach of profiling the application code.