SPRADN4 December 2024 AM62P , AM62P-Q1
Most of the processor IOs are not fail-safe. For information on fail-safe IOs, see the processor-specific data sheet. Power the IO supply of attached devices from the same power source as the respective processor dual-voltage IO groups (VDDSHVx supply rail) to verify that the system never applies potential to an IO that is not powered. Taking care of fail-safe operation is recommended to protect the IOs of processor and attached devices.
For more information on power-sequencing requirements between processor and attached devices including signal isolation for fail-safe operation, see [FAQ] AM625 / AM623 Custom board hardware design – Power sequencing between SOC (Processor) and the Attached devices. The FAQ is generic and can also be used for AM62P, AM62P-Q1 processor family.
Verify that a valid supply voltage for the VDDSHVx IO supplies is present before applying inputs to the associated processor IOs or peripherals.
Connect the VDDSHVx IO supplies and associated CAP_VDDSn capacitor irrespective of the usage of the processor IOs or peripherals.