SPRADO2B November 2024 – January 2025 AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1
When external inputs drive the boot mode configuration, the recommendation is to stabilize the boot mode configuration inputs before the processor MCU_PORz (cold reset) is released.
When using an Ethernet boot and a Reduced Gigabit Media Independent Interface (RGMII), implement an EPHY into the design that starts RGMII_ID mode on the EPHY RX data path and disables RGMII_ID mode on the TDn data path (the processor implements RGMII_ID on the TDn outputs). Processor ROM does not enable or disable RGMII_ID mode on attached EPHYs programmatically. Typically, RGMII_ID setting is accomplished via pin strapping on the EPHY.
Select a EPHY with the capability to set the RGMII internal delay through a pin strap, see the processor-specific SK. For more information, see the advisory i2329 MDIO: MDIO interface corruption (CPSW and PRU-ICSS) of the processor-specific silicon errata.