SPRADP0 December   2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P4 , AM263P4-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1List of Acronyms
  5. 2Software Setup
  6. 3Hardware Setup
    1. 3.1 AM263x Connections
    2. 3.2 AM263Px Connections
    3. 3.3 Lauterbach® Connections
  7. 4Building MCU_PLUS_SDK Examples
    1. 4.1 CCS Import And Build
    2. 4.2 Command Line Build
  8. 5CMM Scripts
    1. 5.1 AM263x CMM Script
    2. 5.2 AM263Px CMM Script
  9. 6Flashing SBL Null
    1. 6.1 Using UniFlash tool
    2. 6.2 Using Command Line Python Scripts
  10. 7Debugging with Trace32 Software
  11. 8Summary
  12. 9References

AM263Px Connections

The AM263Px schematics differ from the AM263x. As a result, some of the steps can be different in-case of AM263Px.

  1. Dock the AM263Px device on the HSEC Dock breakout board.
  2. Connect the power supply to the HSEC Dock breakout board.
  3. Connect the USB Type-A to micro-B from the Host PC to the AM26x microcontroller.
  4. On the AM263Px, put the SW-1 switch to OFF to disconnect the onboard debugger. Next, put SW-14 switch to OFF, SW-15 switch to OFF and SW-16 switch to ON state. This is necessary to route the signals to the HSEC board to which the Lauterbach trace pins are connected.

    Switch

    State

    SW-1

    Low

    SW-14

    Low

    SW-15

    Low

    SW-16

    High

  5. Power on the HSEC Dock breakout board. LD2, LD4, LD5, LD9 glows on the AM263Px.
 AM263Px PCB# PROC E2
                    Switches Figure 3-3 AM263Px PCB# PROC E2 Switches
 AM263Px Control Card Mounted
                    on HSEC Dock Board Figure 3-4 AM263Px Control Card Mounted on HSEC Dock Board