SPRU514Z July 2001 – October 2023 SM320F28335-EP
You can invoke mklib directly to build any or all of the libraries indexed in the index library libc.a. The libraries are built with the standard options for that library; the library names and the appropriate standard option sets are known to mklib.
This is most easily done by changing the working directory to be the compiler run-time-support library directory 'lib' and invoking the mklib executable there:
mklib --pattern=rts2800_ml.lib
For C28x these are some of the libraries can be built. See Section 8.1.8 for the full RTS library naming options.