SPRUGR9H November 2010 – April 2015 66AK2E05 , 66AK2H06 , 66AK2H12 , 66AK2H14 , 66AK2L06 , AM5K2E02 , AM5K2E04 , SM320C6678-HIREL , TMS320C6652 , TMS320C6654 , TMS320C6655 , TMS320C6657 , TMS320C6670 , TMS320C6671 , TMS320C6672 , TMS320C6674 , TMS320C6678
When a channel is first started, the PDSP owns both the ping and pong pages in host processor memory. When a page is filled by the PDSP, an interrupt is sent to the host. This tells the host that the PDSP wants it to take ownership of the page. This interrupt should be acknowledged by the host as quickly as possible to enable ownership of the page. After the interrupt is acknowledged, the host retains ownership of the page until a second interrupt firing and acknowledgement occurs.
Figure 4-1 shows the handshaking that occurs between the accumulator firmware, the INTD and the host software during processing of descriptor lists: