SPRUHJ1I January 2013 – October 2021 TMS320F2802-Q1 , TMS320F28026-Q1 , TMS320F28026F , TMS320F28027-Q1 , TMS320F28027F , TMS320F28027F-Q1 , TMS320F28052-Q1 , TMS320F28052F , TMS320F28052F-Q1 , TMS320F28052M , TMS320F28052M-Q1 , TMS320F28054-Q1 , TMS320F28054F , TMS320F28054F-Q1 , TMS320F28054M , TMS320F28054M-Q1 , TMS320F2806-Q1 , TMS320F28062-Q1 , TMS320F28062F , TMS320F28062F-Q1 , TMS320F28068F , TMS320F28068M , TMS320F28069-Q1 , TMS320F28069F , TMS320F28069F-Q1 , TMS320F28069M , TMS320F28069M-Q1
Even though recalibration takes time to execute, it is recommended to always enable both Offset Recalibration and Rs Recalibration to make sure the parameters are more accurate before running the motor, especially if the motor has been in idle for a long time. If the motor has not been run by the code for long periods of time, it is likely that ambient temperature affects the stator resistance of the motor, so Rs recalibration is recommended. Board offset recalibration is not as critical since it is hardware dependent, however, longevity of passive components and temperature variations could potentially affect the hardware offsets, so it is recommended that these offsets are tuned periodically.