SPRUHJ1I January 2013 – October 2021 TMS320F2802-Q1 , TMS320F28026-Q1 , TMS320F28026F , TMS320F28027-Q1 , TMS320F28027F , TMS320F28027F-Q1 , TMS320F28052-Q1 , TMS320F28052F , TMS320F28052F-Q1 , TMS320F28052M , TMS320F28052M-Q1 , TMS320F28054-Q1 , TMS320F28054F , TMS320F28054F-Q1 , TMS320F28054M , TMS320F28054M-Q1 , TMS320F2806-Q1 , TMS320F28062-Q1 , TMS320F28062F , TMS320F28062F-Q1 , TMS320F28068F , TMS320F28068M , TMS320F28069-Q1 , TMS320F28069F , TMS320F28069F-Q1 , TMS320F28069M , TMS320F28069M-Q1
One of the considerations when operating at low speeds is that the speed controller must be tuned to avoid the motor stalling. The SpinTAC speed controller provided in InstaSPIN-MOTION is an advanced speed controller that provides a single parameter tuner and a wide operating range. These combine to make it easy to tune the SpinTAC speed controller to avoid motor stall when operating at low speed. The one important note when tuning the SpinTAC speed controller for low speed operations is that the Bandwidth might need to be set higher than for rated speed operations. This needs to be done so that the SpinTAC speed controller will act more aggressivly to cancel disturbances and regulate low speeds. More information about the SpinTAC speed controller provided in InstaSPIN-MOTION can be found in Section 13.