SPRUHX5I August 2014 – May 2024 TMS320F28374S , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378S , TMS320F28379S
File | Driverlib Function |
---|---|
CAN_CTL | |
can.c | CAN_initModule |
can.c | CAN_setBitTiming |
can.h | CAN_startModule |
can.h | CAN_enableController |
can.h | CAN_disableController |
can.h | CAN_enableTestMode |
can.h | CAN_disableTestMode |
can.h | CAN_setInterruptionDebugMode |
can.h | CAN_disableAutoBusOn |
can.h | CAN_enableAutoBusOn |
can.h | CAN_enableInterrupt |
can.h | CAN_disableInterrupt |
can.h | CAN_enableRetry |
can.h | CAN_disableRetry |
can.h | CAN_isRetryEnabled |
CAN_ES | |
can.c | CAN_clearInterruptStatus |
can.h | CAN_getStatus |
CAN_ERRC | |
can.h | CAN_getErrorCount |
CAN_BTR | |
can.c | CAN_setBitTiming |
can.h | CAN_getBitTiming |
CAN_INT | |
can.h | CAN_getInterruptCause |
CAN_TEST | |
can.h | CAN_enableTestMode |
can.h | CAN_disableTestMode |
can.h | CAN_enableMemoryAccessMode |
can.h | CAN_disableMemoryAccessMode |
CAN_PERR | |
- | |
CAN_RAM_INIT | |
can.h | CAN_initRAM |
CAN_GLB_INT_EN | |
can.h | CAN_enableGlobalInterrupt |
can.h | CAN_disableGlobalInterrupt |
CAN_GLB_INT_FLG | |
can.h | CAN_getGlobalInterruptStatus |
CAN_GLB_INT_CLR | |
can.h | CAN_clearGlobalInterruptStatus |
CAN_ABOTR | |
can.h | CAN_setAutoBusOnTime |
CAN_TXRQ_X | |
- | |
CAN_TXRQ_21 | |
can.h | CAN_getTxRequests |
CAN_NDAT_X | |
- | |
CAN_NDAT_21 | |
can.h | CAN_getNewDataFlags |
CAN_IPEN_X | |
- | |
CAN_IPEN_21 | |
can.h | CAN_getInterruptMessageSource |
CAN_MVAL_X | |
- | |
CAN_MVAL_21 | |
can.h | CAN_getValidMessageObjects |
CAN_IP_MUX21 | |
can.h | CAN_getInterruptMux |
can.h | CAN_setInterruptMux |
CAN_IF1CMD | |
can.c | CAN_clearInterruptStatus |
can.c | CAN_setupMessageObject |
can.c | CAN_sendMessage |
can.c | CAN_sendMessage_16bit |
can.c | CAN_sendMessage_32bit |
can.c | CAN_sendMessage_updateDLC |
can.c | CAN_sendRemoteRequestMessage |
can.c | CAN_transferMessage |
can.c | CAN_clearMessage |
can.c | CAN_disableMessageObject |
can.c | CAN_disableAllMessageObjects |
CAN_IF1MSK | |
can.c | CAN_setupMessageObject |
CAN_IF1ARB | |
can.c | CAN_setupMessageObject |
can.c | CAN_clearMessage |
can.c | CAN_disableMessageObject |
can.c | CAN_disableAllMessageObjects |
CAN_IF1MCTL | |
can.c | CAN_setupMessageObject |
can.c | CAN_sendMessage |
can.c | CAN_sendMessage_16bit |
can.c | CAN_sendMessage_32bit |
can.c | CAN_sendMessage_updateDLC |
can.c | CAN_sendRemoteRequestMessage |
CAN_IF1DATA | |
can.c | CAN_sendMessage |
can.c | CAN_sendMessage_16bit |
can.c | CAN_sendMessage_32bit |
can.c | CAN_sendMessage_updateDLC |
CAN_IF1DATB | |
- | See IF1DATA |
CAN_IF2CMD | |
can.c | CAN_readMessage |
can.c | CAN_transferMessage |
CAN_IF2MSK | |
- | |
CAN_IF2ARB | |
can.c | CAN_readMessageWithID |
CAN_IF2MCTL | |
can.c | CAN_readMessage |
CAN_IF2DATA | |
can.c | CAN_readMessage |
CAN_IF2DATB | |
- | See IF2DATA |
CAN_IF3OBS | |
- | |
CAN_IF3MSK | |
- | |
CAN_IF3ARB | |
- | |
CAN_IF3MCTL | |
- | |
CAN_IF3DATA | |
- | |
CAN_IF3DATB | |
- | See IF3DATA |
CAN_IF3UPD | |
- |