SPRUHX5I August 2014 – May 2024 TMS320F28374S , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378S , TMS320F28379S
If a frame-synchronization pulse starts the transfer of a new frame before the current frame is fully transmitted, this pulse is treated as an unexpected frame-synchronization pulse.
When XFIG = 1, normal transmission continues with unexpected frame-synchronization signals ignored.
When XFIG = 0 and an unexpected frame-synchronization pulse occurs, the serial port:
For more details about the frame-synchronization error condition, see Section 20.5.6.