SPRUHX5I August 2014 – May 2024 TMS320F28374S , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378S , TMS320F28379S
Hibernate is a chip-level low-power mode that gates power to large portions of the device. Waking up from hibernate involves a special reset (HIBRESET). This reset is similar to a POR except that the I/O pins remain isolated and the XRS pin is not toggled. (An external XRS toggle during hibernate triggers a HIBRESET). I/O isolation is disabled in software as part of a special boot ROM flow. For more information on hibernate, refer to Section 3.10.
After a hibernate reset, the HIBRESETn bit in RESC is set. This bit is then cleared by the boot ROM.