SPRUHX5I August 2014 – May 2024 TMS320F28374S , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378S , TMS320F28379S
For a shared RAM, multiple accesses can happen at a given time. The maximum number of accesses to any shared RAM at any given time depends on the type of shared RAM. On this device, a combination of a fixed and round robin scheme is followed to arbitrate multiple access at any given time.
The following is the order of fixed priority for CPU accesses:
The following is the order of fixed priority for CLA accesses:
Figure 3-15 represents the arbitration scheme on global shared memories:
Figure 3-16 represents the arbitration scheme on local shared memories.