When the receiver FIFO is enabled in the FIFO control register (FCR), mapped in the MSB part of the register PRUSS_UART_INTERRUPT_IDENTIFICATION_REGISTER_FIFO_CONTROL_REGISTER, and the receiver interrupts are enabled in the interrupt enable register PRUSS_UART_INTERRUPT_ENABLE_REGISTER, the interrupt mode is selected for the receiver FIFO. The following are important points about the receiver interrupts:
- The receiver data-ready interrupt is issued to the CPU when the FIFO has reached the trigger level that is programmed in FCR. It is cleared when the CPU or the DMA controller reads enough characters from the FIFO such that the FIFO drops below its programmed trigger level.
- The receiver line status interrupt is generated in response to an overrun error, a parity error, a framing error, or a break. This interrupt has higher priority than the receiver data-ready interrupt. For details, see Section 30.7.3.4.
- The data-ready (DR) bit in the line status register (LSR) - PRUSS_UART_LINE_STATUS_REGISTER, indicates the presence or absence of characters in the receiver FIFO. The DR bit is set when a character is transferred from the receiver shift register (RSR) to the empty receiver FIFO. The DR bit remains set until the FIFO is empty again.
- A receiver time-out interrupt occurs if all of the following conditions exist:
- At least one character is in the FIFO,
- The most recent character was received more than four continuous character times ago. A character time is the time allotted for 1 START bit, n data bits, 1 PARITY bit, and 1 STOP bit, where n depends on the word length selected with the WLS0 and WLS1 bits of the line control register PRUSS_UART_LINE_CONTROL_REGISTER. See Table 30-226.
- The most recent read of the FIFO has occurred more than four continuous character times before.
- Character times are calculated by using the baud rate.
- When a receiver time-out interrupt has occurred, it is cleared and the time-out timer is cleared when the CPU or the EDMA controller reads one character from the receiver FIFO. The interrupt is also cleared if a new character is received in the FIFO or if the URRST bit is cleared in the power and emulation management register PRUSS_UART_POWERMANAGEMENT_AND_EMULATION_REGISTER.
- If a receiver time-out interrupt has not occurred, the time-out timer is cleared after a new character is received or after the CPU or EDMA reads the receiver FIFO.
When the transmitter FIFO is enabled in PRUSS_UART_INTERRUPT_IDENTIFICATION_REGISTER_FIFO_CONTROL_REGISTER [0] IPEND_FIFOEN bit and the transmitter holding register empty (THRE) interrupt is enabled in PRUSS_UART_INTERRUPT_ENABLE_REGISTER[1] ETBEI bit, the interrupt mode is selected for the transmitter FIFO. The THRE interrupt occurs when the transmitter FIFO is empty. It is cleared when the transmitter hold register (THR) PRUSS_UART_RBR_THR_REGISTERS [7:0] DATA bitfield is loaded (1 to 16 characters may be written to the transmitter FIFO while servicing this interrupt) or the interrupt identification register INTID bitfield is read in the PRUSS_UART_INTERRUPT_IDENTIFICATION_REGISTER_FIFO_CONTROL_REGISTER.
Table 30-226 Character Time for Word LengthsWord Length (n) | Character Time | Four Character Times |
---|
5 | Time for 8 bits | Time for 32 bits |
6 | Time for 9 bits | Time for 36 bits |
7 | Time for 10 bits | Time for 40 bits |
8 | Time for 11 bits | Time for 44 bits |