SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
The statistics collector module implements a suspend input that is used to avoid statistics collector counters to be updated while the processor has entered the debug state. This avoids triggering false alerts upon execution resume. When the statistics collector is asserted to 1, it freezes the monitoring process. When it goes back to 0, the monitoring resumes. If a frame is being dumped, it will not be stopped by suspend.
Each statistic collector has an ignore suspend register, which can be used to disable the suspend feature.