SPRUI04F july 2015 – april 2023
The compiler supports the 2011 standard of C as standardized by the ISO. However, in addition to the list in Section 7.13.1, the following run-time functions and features are not implemented or fully supported in C11 mode: