When recompiling with --use_profile_info, the profile information is invalid in the following cases:
- The source file name changed between the generation of profile information (gen-profile) and the use of the profile information (use-profile).
- Source code was modified since gen-profile. In
this case, profile information is invalid for modified functions.
- Certain compiler options used with gen-profile are different from those with used with use-profile. In particular, options that affect parser behavior could invalidate profile data during use-profile. In general, using different optimization options during use-profile should not affect the validity of profile data.