See
the following resources for further information
about the TI Code Generation Tools:
You
can use the following documents to supplement this
user's guide:
SPRUI03
TMS320C6000 Assembly Language Tools
User's Guide. Describes the assembly
language tools (assembler, linker, and other tools
used to develop assembly language code), assembler
directives, macros, common object file format, and
symbolic debugging directives for the C64+, C6740,
and C6600 variants of the TMS320C6000 platform of
devices. Refer to SPRU186 when using legacy
C6200, C6400, C6700, and C6700+ devices.
SPRAB89
The C6000 Embedded Application Binary
Interface. Provides a specification for
the ELF-based Embedded Application Binary
Interface (EABI) for the TMS320C6000 family of
processors from Texas Instruments. The EABI
defines the low-level interface between programs,
program components, and the execution environment,
including the operating system if one is
present.
SPRU190
TMS320C6000 DSP Peripherals Overview
Reference Guide. Provides an overview and
briefly describes the peripherals available on the
TMS320C6000 family of digital signal processors
(DSPs).
SPRU732
TMS320C64x/C64x+ DSP CPU and Instruction
Set Reference Guide. Describes the CPU
architecture, pipeline, instruction set, and
interrupts for the TMS320C64x and TMS320C64x+
digital signal processors (DSPs) of the
TMS320C6000 DSP family. The C64x/C64x+ DSP
generation comprises fixed-point devices in the
C6000 DSP platform. The C64x+ DSP is an
enhancement of the C64x DSP with added
functionality and an expanded instruction
set.
SPRUGH7
TMS320C66x CPU and Instruction Set
Reference Guide. Describes the CPU
architecture, pipeline, instruction set, and
interrupts for the TMS320C66x digital signal
processors (DSPs) of the TMS320C6000 DSP platform.
The C66x DSP generation comprises floating-point
devices in the C6000 DSP platform.
SPRUFE8
TMS320C674x CPU and Instruction Set
Reference Guide. Describes the CPU architecture, pipeline, instruction set,
and interrupts for the TMS320C674x digital signal processors (DSPs) of the TMS320C6000
DSP platform. The C674x is a floating-point DSP that combines the TMS320C67x+ DSP and
the TMS320C64x+ DSP instruction set architectures into one core.
SPRAAB5
The Impact of DWARF on TI Object
Files.
Describes the Texas Instruments extensions to the
DWARF specification.
SPRUEX3
TI SYS/BIOS Real-time Operating System
User's Guide. SYS/BIOS gives application
developers the ability to develop embedded
real-time software. SYS/BIOS is a scalable
real-time kernel. It is designed to be used by
applications that require real-time scheduling and
synchronization or real-time instrumentation.
SYS/BIOS provides preemptive multithreading,
hardware abstraction, real-time analysis, and
configuration tools.