SPRUI33H November 2015 – June 2024 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
FILE: fsi_ex2_loopback_clacontrol.c
Example sets up infinite data frame transfers where trigger happens through CLA. Automatic(Hw triggered) Ping frame transmission is also setup along with data. This example is similar to fsi_ex1_loopback_cpucontrol and only different in in the sense that data frame transfer are trigged from a CLA task. Using CLA will release some of load from CPU and help it in providing time for other tasks.
User can edit some of configuration parameters as per usecase. These are as below. Default values can be referred in code where these globals are defined
For any errors during transfers i.e. error events such as Frame Overrun, Underrun, Watchdog timeout and CRC/EOF/TYPE errors, execution will stop immediately and status variables can be looked into for more details. Execution will also stop for any mismatch between received data and sent ones and also if transfers takes unusually long time(detected through software counters - txTimeOutCntr and rxTimeOutCntr)
External Connections
For FSI internal loopback (EXTERNAL_FSI_ENABLE == 0), no external connections needed
For FSI external loopback (EXTERNAL_FSI_ENABLE == 1), external connections are required. The FSI TX pins should be connected to the respective FSI RX pins of the same device. See below for external connections to include and GPIOs used:
External Connections Required between FSI TX and RX of the same device:
ControlCard FSI Header GPIOs:
LaunchPad FSI Header GPIOs:
Watch Variables