SPRUI33H November 2015 – June 2024 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
Table 3-3 shows the PIE group and channel assignments for each peripheral interrupt. Each row is a group, and each column is a channel within that group. When multiple interrupts are pending, the lowest-numbered channel is the lowest-numbered group is serviced first. Thus, the interrupts at the top of the table have the highest priority, and the interrupts at the bottom have the lowest priority.
INTx.1 | INTx.2 | INTx.3 | INTx.4 | INTx.5 | INTx.6 | INTx.7 | INTx.8 | INTx.9 | INTx.10 | INTx.11 | INTx.12 | INTx.13 | INTx.14 | INTx.15 | INTx.16 | |
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
INT1.y | ADCAINT1 | ADCBINT1 | ADCCINT1 | XINT1 | XINT2 | - | TIMER0 | WAKE | - | - | - | - | - | - | - | - |
INT2.y | EPWM1_TZINT | EPWM2_TZINT | EPWM3_TZINT | EPWM4_TZINT | EPWM5_TZ | EPWM6T_TZ | EPWM7_TZ | EPWM8_TZ | - | - | - | - | - | - | - | - |
INT3.y | EPWM1_INT | EPWM2_INT | EPWM3_INT | EPWM4_INT | EPWM5_INT | EPWM6 | EPWM7 | EPWM8 | - | - | - | - | - | - | - | - |
INT4.y | ECAP1 | ECAP2 | ECAP3 | ECAP4 | ECAP5 | ECAP6 | ECAP7 | - | - | - | - | - | - | ECAP6INT2 | ECAP7INT2 | - |
INT5.y | EQEP1_INT | EQEP2_INT | - | - | CLB1_INT | CLB2_INT | CLB3_INT | CLB4_INT | SD1FLT1_DRINT | - | - | - | SD1FLT1_DRINT | SD1FLT2_DRINT | SD1FLT3_DRINT | SD1FLT4_DRINT |
INT6.y | SPIA_RX | SPIA_TX | SPIB_RX | SPIB_TX | - | - | - | - | - | - | - | - | - | - | - | - |
INT7.y | DMA_CH1INT | DMA_CH2INT | DMA_CH3INT | DMA_CH4INT | DMA_CH5INT | DMA_CH6 | - | - | - | - | FSITXA_INT1 | FSITXA_INT2 | FSIRXA_INT1 | FSIRXA_INT2 | CLA1PROMCRC | DCC0_INT |
INT8.y | I2CA_INT | I2CA_FIFO | - | - | - | - | - | - | LINA_INT0 | LINA_INT1 | - | - | PMBUSA | - | - | - |
INT9.y | SCIA_RX | SCIA_TX | SCIB_RX | SCIB_TX | DCANA_INT1 | DCANA_INT2 | DCANB_INT1 | DCANA_INT2 | - | - | - | - | - | - | - | - |
INT10.y | ADCA_EVT | ADCAINT2 | ADCAINT3 | ADCAINT4 | ADCB_EVT | ADCBINT2 | ADCBINT3 | ADCBINT4 | ADCC_EVT | ADCC2 | ADCC3 | ADCC4 | - | - | - | - |
INT11.y | CLA1_1 | CLA1_2 | CLA1_3 | CLA1_4 | CLA1_5 | CLA1_6 | CLA1_7 | CLA1_8 | - | - | - | - | - | - | - | - |
INT12.y | XINT3 | XINT4 | XINT5 | PBIST | FMC_INT | - | FPU_OVFINT | FPU_UNFINT | - | RAM_CORRECTABLE_ERR | FLASH_CORRECTABLE_ERR | RAM_ACC_VIOL | SYS_PLL_SLIP | BGCRC_CLA1 | CLA_LVF | CLA_LUF |