SPRUI33H November 2015 – June 2024 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
The device has a watchdog timer that can optionally trigger a reset if the watchdog timer is not serviced by the CPU within a user-specified amount of time. This watchdog reset (WDRS) produces an XRS that lasts for 512 INTOSC1 cycles.
After a watchdog reset, the WDRSn bit in RESC is set. If both the XRSn and WDRSn bits are set in RESC, then the reset was initiated by the watchdog. If only the XRSn bit is set in RESC, then the watchdog is a reset from XRSn.