SPRUI76B March 2017 – June 2022 TMS320F28379D , TMS320F28379D-Q1
The Delfino F28379D controlCARD (TMDSCNCD28379D) from Texas Instruments (TI) provides a great way to learn and experiment with the F2837x device family within TI’s C2000™ family of microcontrollers (MCUs). This 180-pin controlCARD is intended to provide a well-filtered robust design that is capable of working in most environments. This document provides the hardware details of the F28379D controlCARD and explains the functions, locations of jumpers, and connectors present on the board.
Delfino, C2000™, and Code Composer Studio™ are trademarks of Texas Instruments.
All trademarks are the property of their respective owners.
As of January 2016, all kits based on the F28377D MCU will now be replaced with the new F28379D superset device. These two MCUs are identical except for the addition of the CLB on the F28379D MCU to enable Position Manager. If the CLB is not a requirement in your application, that feature can be left untouched and the MCU will perform like the F28377D.
Each controlCARD comes with a Hardware Developer’s Kit, a full set of files necessary to evaluate and develop with a C2000 device. These files include:
The Hardware Developer's Kit for the controlCARD can be found in the C2000Ware at the following location:
This kit is designed to explore the functionality of the F2837x microcontrollers. Even though the controlCARD can be treated as a good reference design, it is not intended to be a complete customer design. Full compliance to safety, EMI/EMC, and other regulations are left to the designer of the final customer’s system.
Current revision of controlCARD as of 2-Oct-2015: PCB rev - R1.3, ASSY rev - B.
The Letter B on the controlCARD's Serial Number sticker denotes ASSY rev – B.