SPRUIG8J January 2018 – March 2024
The copy table format is the same irrespective of the compression_kind. The size field of the copy record is overloaded to support compression. Figure 12-4 illustrates the compressed copy table layout.
In Figure 12-4, if the size in the copy record is non-zero it represents the size of the data to be copied, and also means that the size of the load data is the same as the run data. When the size is 0, it means that the load data is compressed.