SPRUII1A November 2017 – January 2020
The Fusion board is designed to match the size of various processor EVMs, such as the TDA2xEco or TDA2Px EVM. The TDA2Px processor is designed for automotive ADAS and self-driving car applications. The board size of the TDA3x EVM is larger than the EVMs previously mentioned, but the mounting holes are placed in the same position on all the boards, to maintain overall compatibility. Similarly, the Fusion board can interface with the TDA4 EVM, mounted of to the side of the EVM. The Fusion board can also connect to a J6Eco, J6Entry, or other EVMs with the same connector. An additional SAMTEC HQCD connector cable is needed to connect to the J6Eco or J6Entry. As a result, the connection between the board and the EVM must be in a fixed position too.