SPRUIL1D May 2019 – December 2024 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
If a single PVU cannot support the required bandwidth, then multiple PVU instances must be used. Since the PVU does not have any address decode, using an IPA, then any splitting is done based on the bus orderid value. That means the peripherals accessing the PVU must be set to use the correct orderid so that they are routed to the correct PVU.