SPRUIL1D May 2019 – December 2024 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
Figure 6-74 shows the Timer Manager diagram.
The 1024 timers in the timer manager are organized as the Timer RAM in Figure 11-7. When the timer manager is enabled, the timer counter will increment with the input timer tick, and the control module continuously loops over the Timer RAM, comparing the values against this timer count. When the timer count is greater than a timer value, the timer control module will generate a timer expiration event.
Based on software writes, the timer control module will update the values in the Timer RAM to setup or cancel active timers. Whenever a new value is written to a TIMERMGR_SETUP_j_k memory address, the corresponding timer is touched/setup with the current sum of the timer count and the written value; written values are relative to the current timer count. These values are stored in the Timer Reprogramming RAM, so the software may also write to the TIMERMGR_CONTROL_j_k registers to flag a timer for reprogramming, using the previously stored reprogramming value. The latter method is preferred when the timer setup value is not changing, as it does not interrupt the RAM state machine.