SPRUIL1D May 2019 – December 2024 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
In order to provide higher security level an optional Km-key encryption is provided. If Km-key encryption is enabled while sending HDCP_TX_CONFIGURATION command, then HDCP controller will expect Master Key, 1.4 Device Keys and Global Constant. These keys will be decrypted using Km-key (loaded using HDCP2_TX_SET_KM_KEY_PARAMS command) by the controller’s internal Firmware and used during Authentication and Key Exchange procedure. The Km-key encryption will also assure that when host reads Master Key it will receive it in encrypted form.
Enabling Km-key encryption affects the following commands or their parameters: