SPRUIL2A February 2019 – September 2019 OMAP-L132 , OMAP-L138 , TMS320C6742 , TMS320C6746 , TMS320C6748
Arm is a registered trademark of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
All other trademarks are the property of their respective owners.
The LCDK is an easy-to-use, affordable and scalable introduction to the world of TI's C6000 DSP value line family. Beginners and experienced users alike can use the kit to create low-power and low-cost solutions for biometrics, analytics, audio, and communications.
TI provides two variants of LCDK, LCDK6748 for DSP only developers and LCDKL138 for Arm® and DSP developers.
For more information, see the following:
NOTE
Steps to Get Started | TMDSLCDK6748 | TMDSLCDK138 |
---|---|---|
Take a tour of the hardware | Introduction to TMDSLCDK6748 | Introduction to TMDSLCDKL138 |
Run out of the box demo | Video Training | Video training |
Software download | Processor SDK OMAPL138 | Processor SDK OMAPL138 |
Hardware setup | TMDSLCDK6748 Hardware setup | TMDSLCDKL138 Hardware Setup |
RTOS software setup | Processor SDK RTOS Getting Started Guide | |
OMAP-L138/C6748 LCDK Hardware Setup with CCS | ||
Linux softwaresetup | Not applicable | Processor SDK Linux Getting Started Guide |
Tool | Order Today |
---|---|
LCDK | C6748-LCDK |
OMAP-L138 LCDK | |
Emulators | XDS100 |
Visit the online TI store for an up-to-date list of available emulators. | XDS200 |
XDS510 | |
XDS560 | |
XDS110 - Supported on C6748 LCDK ONLY |
NOTE
Included Devices | Description | Documentation |
---|---|---|
TMS320C6748 | TMS320C6748 Fixed/Floating Point DSP | TMS320C6748™ Fixed- and Floating-Point DSP Data Sheet |
OMAPL138 | OMAPL138 DSP+ARM9 Processor | OMAP-L138 C6000™ DSP+ ARM® Processor Data Sheet |
Compiler/Debugger (IDE) | Download Now! |
---|---|
Code Composer Studio (CCS) | Download Now (Requires TI Login) |
Processor SDK (Latest) | Download Now (Requires TI Login) |