SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
Split TR mode channels can experience an incoming packet whose length is shorter than what was expected based on one or more TRs which form the control description for the expected packet. If an EOP is received for a TR and the TR has not been completely executed, the port is required to receive as much data as is actually provided in the incoming data placing it in accordance with the instructions in the TR and the to continue executing any remaining TR(s) such that the required events are produced to keep downstream consumers in sync. In this case, no data will be transferred to the buffers described by the TR beyond what was provided in the incoming packet.