SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The only blocking condition is caused when the VBUSM command/data FIFO is full. It is required that the external bandwidth is very high. All egress commands and data should get sent without head of line blocking. Based on arbitration some delay is possible.