SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
In this mode, the ROM Code configures the GPMC interface based on the configuration parameters specified in the boot parameter table for the GPMC NOR boot mode. The boot parameter structure definition for the GPMC NOR boot mode and the parts of this table that can be configured by the BOOTMODE pins are detailed in Section 4.4.9, GPMC NOR Boot Device Configuration.