SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
GPMC NOR boot mode is not executable-in-place (XIP). ROM code first copies boot image into on-chip RAM and then executes it. If the initial image at offset 0x0 is not recognized, the ROM will attempt to read a redundant image from offset 0x100000. This is the only redundant image supported by the ROM.