SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The A53SS does not have an integrated watchdog timer. Instead, this feature is provided externally by the Real Time Interrupt Module (RTI) module, which implements a windowed watchdog timer capable of issuing warm reset to the SoC, when necessary.
There are two RTI modules in the MAIN Domain, which are assigned to the A53 cores as follows:
For more details on the RTI windowed watchdog feature, see Section 12.5.2, Real Time Interrupt Module (RTI/WWDT).