SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
Since the TR mode engine performs transfer sequencing using a count based mechanism it is susceptible to becoming out of synchronization if the source of the data and the destination for the data do not exactly match in their expectations for how much data will be transferred. The following sections outline these scenarios.
TR mode channel exceptions include:
Reception of EOL delimiter
Short Packets
Long Packets
Descriptor Starvation