SPRUIM6A October 2018 – November 2020
The following modifications are needed for PHY2 (U4) to convert it for use with the MII interface.
Clock modification – The clock resistors for U4 is on the bottom of the board. Remove R456 and install a zero ohm resistor in the footprint for R457 as shown in Figure 7-5.
Configuration modification – The circuit for U4 is on the top of the board. Add three zero ohm 0402 resistors to R449, R378, and R448 to configure the interface for MII.