SPRUIM6A October 2018 – November 2020
HFOSC0, HFOSC1: The HFOSC0 (OSC0) and HFOSC1 (OSC1) clocks are muxed inside the SOC, and the result is connected to main PLL. The output of the main PLL is used as the system clock for SOC. The input of WKUP_OSC 0 can be provided with a 25-Mhz crystal or by using the output of the clock generator. The default 25-Mhz crystal is connected; to use the clock generator output as input for WKUP_OSC 0, resistor R448 must be mounted and resistors R450 and R457 removed.
LFOSC: The 32.768-KHz square wave is provided by the MFP output of the RTC component.