SPRUIT5 April 2021 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
As indicated in Figure 4-5, ERRORSTS pin is an integral part of MCU safety concept used for indicating to an external system about a critical error occurring within in the MCU. Proper functioning of ERRORSTS pin and error handling of the system external to MCU can be checked by asserting ERRORSTS pin by generating an error condition using one of the software provided ways (asserting CLOCLKFAIL NMIFLG by updating the NMIFLGFRC.bit.CLOCKFAIL). Error response, diagnostic testability, and any necessary system requirements are defined by the system integrator.