SPRUIT8D February 2020 – February 2021 AWR2243
Connectivity is provided using the micro USB connector over the onboard XDS110 (TM4C1294NCPDT) emulator. This connection provides the following interfaces to the PC:
When the USB is connected to the PC the device manager recognizes the following COM ports, as shown in Figure 2-8:
If Windows® is unable to recognize the COM ports previously shown, install the emupack available here