SPRUIV7B May 2022 – September 2023 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
Most peripherals which are serviced by the Peripheral DMA follow the pattern of transferring X bytes from a fixed, non-changing address in a loop Y times for each triggering event that is received. The X parameter is typically 1-16 bytes and the Y parameter can be any integer up to 2048. If a peripheral can be serviced by this basic functionality then it is recommended to use this mode for the peripheral.