SPRUIV7B May 2022 – September 2023 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
In the unlikely event that channel synchronization is corrupted, a channel may fail to teardown gracefully, even with flush enabled. If this occurs, the channel may be reset by clearing the enable bit in the PSI-L Enable register. This will cause a local reset of the entire channel, including TR and pairing registers. Note that it does not reset the UDMA-P peer. Resetting the UDMA-P peer is also required before re-initializing and re-pairing the channel.