SPRUIV7B May 2022 – September 2023 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
To assign a receiver to a mailbox, set the new message interrupt enable bit corresponding to the desired mailbox in the MAILBOX_IRQ_ENABLE_SET_j register. The receiver reads the MAILBOX_MESSAGE_y register to retrieve a message from the mailbox.
An alternate method for the receiver that does not use the interrupts is to poll the MAILBOX_FIFO_STATUS_y and/or MAILBOX_MSG_STATUS_y registers to know when to send or retrieve a message to or from the mailbox. This method does not require assigning a receiver to a mailbox. Because this method does not include the explicit assignment of the mailbox, the software must avoid having multiple receivers use the same mailbox, which can result in incoherency.
To assign a sender to a mailbox, set the queue-not-full interrupt enable bit of the desired mailbox in the MAILBOX_IRQ_ENABLE_SET_j register, where u is the number of the sending user. However, direct allocation of a mailbox to a sender is not recommended because it can cause the sending processor to be constantly interrupted.
It is recommended that register polling be used to:
The sender might use the queue-not-full interrupt when the initial mailbox status check indicates the mailbox is full. In this case, the sender can enable the queue-not-full interrupt for its mailbox in the appropriate MAILBOX_IRQ_ENABLE_SET_j register. This allows the sender to be notified by interrupt only when a FIFO queue has at least one available entry.
Reading the MAILBOX_IRQ_STATUS_CLR_j register determines the status of the new message and the queue-not-full interrupts for a particular user. Writing 1 to the corresponding bit in the MAILBOX_IRQ_STATUS_CLR_j register acknowledges, and subsequently clears, an interrupt.
Assigning multiple senders or multiple receivers to the same mailbox is not recommended.