SPRUIV7B May 2022 – September 2023 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
In this mode, the Main Domain I2C0 peripheral is configured as I2C controller.
ROM Code will start reading from the I2C EEPROM at the specified I2C bus address. This read will be done beginning at the specified base address offset. Data will be read in 2-KB chunks. The data will be stored at the address specified in the boot header. It will continue reading image data until a complete image has been read. When the complete image has been read, the ROM Code will branch to the start address of the image.