SPRUIV7B May 2022 – September 2023 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
The ECAP module represents one complete capture channel, which has the following independent key resources:
Multiple identical ECAP modules can be contained in a system as shown in Figure 12-300. For actual number of the ECAP modules integrated in the device, refer to ECAP Integration. The letter x within a signal or module name is used to indicate a generic ECAP instance on a device. For example, output interrupt request, ECAP1INT belongs to ECAP1, ECAP2INT belongs to ECAP2, and so forth.