SPRUIV7B May 2022 – September 2023 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
There are 3 specific errors which may be encountered during Tx split operation and which are trapped by the BCDMA. The following table lists the errors and how the BCDMA will process them:
Condition | Pauses Channel | Error Flag Set in Channel | Data Transfer | TR Flush | Outputs Transfer Events |
---|---|---|---|---|---|
TR null icnt0 | Selectable(1) | Yes | No | Just that TR | No |
Unsupported TR Type |
Selectable(1) | Yes | No | Just that TR | No |
Bus Errors |
Selectable(1) | Yes | Yes | No | Yes |