SPRUIW7A October 2020 – February 2022
There is a DIP switch provided on the J7200 SoM to select the SoC’s DDR and LPDDR4 memory IO supply for the LPDDR4/ LPDDR4x.
The DIP switch SW4 Bit 1 provides an option to change the feedback path of regulator (U49) that decides the output supply voltages.
SW4 Bit 1 | SDRAM_TYPE | Selected DDR IO Voltage |
---|---|---|
OPEN/LOW | LPDDR4 | 1.1 V |
CLOSE/HIGH | LPDDR4x | 0.6 V |
Currently, the J7200 device does not support LPDDR4x. This support may be added at a later date. The EVM does support this feature if/when support is added to the silicon.