SPRUIW7A October 2020 – February 2022
Figure 4-4 shows the power flow and power up sequence for all the discrete supplies on the EVM. Note processor specific power supplies are provided from the Dual PMICs, and its specific power sequence is to support the processor sequence requirements. This sequence is documented in the device-specific processor's data manual. Figure 4-4 illustrates the support of all the other system supplies.