SPRUIW9C October 2021 – March 2024 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
FILE: can_ex8_mask.c
This example initializes CAN module A for Reception. When a frame with a matching filter criterion is received, the data is copied in mailbox 1 and LED is toggled a few times and the code gets ready for the next frame. If a message of any other MSGID is received, an ACK is provided Completion of reception is determined by polling CAN_NDAT_21 register. No interrupts are used. Refer to Programming Examples and Debug Strategies for the DCAN Module for useful information about this example
Hardware Required
Watch Variables