SPRUIW9C October 2021 – March 2024 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
FILE: bgcrc_ex4_clabgcrc_scrubmode.c
This example demonstrates how to configure and trigger CLA-BGCRC in Scrub mode. In Scrub mode, CRC of data is not compared with the golden CRC. Error check is done using the ECC/Parity logic. It also showcases how to configure the CRC watchdog and lock the registers after configuring the module. The watchdog is used as a diagnostic to check memory test completion within the expected time window. An error signal is generated if the test does not complete in the specified time window.
The module is configured for 256 bytes of CLA ROM memory. Interrupt is generated once the computation is done and checks if no error flags are raised. The NMI is enabled and is triggered if an error is detected.
External Connections
Watch Variables