SPRUIW9C October 2021 – March 2024 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
FILE: sdfm_ex5_type1_filter_fifo_cpuread.c
This example configures SDFM1 filter in type 1 to demonstrate data read through CPU in FIFO & non-FIFO mode. Data filter is configured in mode 0 to select SINC3 filter with OSR of 256. Filter output is configured for 16-bit format and data shift of 10 is used.
This example demonstrates the FIFO usage if enabled. FIFO length is set at 16 and data ready interrupt is configured to be triggered when FIFO is full. In this example, SDFM filter data is read by CPU in SDFM Data Ready ISR routine.
External Connections
Watch Variables