SPRUIW9C October 2021 – March 2024 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
FILE: sci_ex4_stdout_redirect.c This test transmits data through the SCI-A port to a terminal
A terminal such as 'putty' can be used to view the data from the SCI. Characters received by the SCI port are sent back to the host.
Running the Application Open a COM port with the following settings using a terminal:
The program will print out three sentences: one to the SCIA, one to CCS, and a final one to SCIA.
External Connections
Connect the SCI-A port to a PC via a transceiver and cable.