SPRUIW9C October 2021 – March 2024 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
The C28x is a little-endian, 16-bit word addressable CPU. Therefore, the 32-bit value of 0x12345678 stored at address 0x100 is stored in the C28x memory as shown in Table 9-2.
Address | 0x100 | 0x101 |
---|---|---|
Data | 0x5678 | 0x1234 |
The BGCRC order of byte calculations of the above example is 0x78, 0x56, 0x34, 0x12 and yields 0x6A330D2D. The 32-bit polynomial 0x04C11DB7 is used with an initialization vector of 0x00000000. The following code snippet shows the effective bit processing. Processing for all 32-bits within a word occurs in a single cycle within the BGCRC hardware.
seed = 0x0UL; //Initialize With Seed
poly = 0x04C11DB7UL: //32-Bit Polynomial
crc32 = seed;
for(i=0; i<dataSize; i++)
{
byteSwappedData = ((data[i] & 0x000000FF) << 24)|
= ((data[i] & 0x0000FF00) << 8) |
= ((data[i] & 0x00FF0000) >> 8) |
= ((data[i] & 0xFF000000) >> 24);
crc32 = byteSwappedData^crc32;
for(j=0; j<32; j++)
{
if(crc32 & 0x80000000) crc32 = (crc32 << 1)^poly;
else crc32 = crc32 << 1;
crc32 = crc32 & 0xFFFFFFFF;
}
}
A second example (Table 9-3) with two 32-bit words, 0x12345678 and 0x9ABCDEF0 at address 0x100 and 0x102 successively, calculates the bytes in the order 0x78, 0x56, 0x34, 0x12, 0xDE, 0xBC, and 0x9A and yield 0x7E0B4164.
Address | 0x100 | 0x101 | 0x102 | 0x103 |
---|---|---|---|---|
Data | 0x5678 | 0x1234 | 0xDEF0 | 0x9ABC |
All data input to the BGCRC must align to a 32-bit boundary, both in the starting address and the size. It is possible to include 16-bit data within the span of data; however, when the data is read by the BGCRC, it always assume 32-bits and conform to the above calculation order. For example, if two 16-bit words (0xA0B1 and 0xC2D3) were placed in between the previous two 32-bit words (Table 9-4), the calculations are performed in byte order 0x78, 0x56, 0x34, 0x12, 0xB1, 0xA0, 0xD3, 0xC2, 0xF0, 0xDE, 0xBC, and 0x9A and yield 0x2AEFD987.
Address | 0x100 | 0x101 | 0x102 | 0x103 | 0x104 | 0x105 |
---|---|---|---|---|---|---|
Data | 0x5678 | 0x1234 | 0xA0B1 | 0xC2D3 | 0xDEF0 | 0x9ABC |